Import Integration - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Menu Selection: Action > Import Integration

This command is only available when an Integration under an engine is selected in the All Items tree. After adding an Integration, you can select the integration in the navigation tree and use this menu selection to add existing devices and points under the integration.