Import Definition - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Action > Import Definition

Imports the pre-built summary definition that is stored on the computer and is only available when the Summary Definitions folder is selected in the All Items tree. After importing a definition, the imported Summary Definitions appear in the Summary Definitions folder in the All Items tree.

Note: You also can import Summary Definitions that were previously exported.