Commanding an Item - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

To send a command to an item in a graphic, see the User Graphics Tool (UGT) section. To send a command to an item in a Graphics+ graphic, see the Graphics+ section. To send a command to multiple items, see the Commanding Multiple Items (Global Command) section.

To command an item:

Procedure

  1. Select the item to command in the navigation tree or in the display panel.
  2. From the Action Menu, select Command, or right-click and select Command.
  3. Filter the list of commands using the Show Command Set drop-down menu, if desired.
  4. Select the command to issue.
    Note: After selecting one of the available commands, you may be prompted to specify additional parameters for the command.
  5. Click Send.
    Note: If an error occurs while sending the command, the dialog box remains open.