Action Menu - Feature Specific - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The following table describes the different menu items that appear in the Action menu based on the active panel or feature displayed in the selected display panel. Click each active panel or feature for a description. For more information on the modes of operation, see Metasys Modes.

Note: The Refresh, Refresh Current Tab, and Refresh All Tabs menu items appear in the Action menu for all other features or active panels.
Table 1. Action Menu - Feature Specific

Active Panel/Feature

Contents In Mode

Online (Standard Access)

Online (Basic Access)

Offline (SCT)

Event Viewer

  • Refresh
  • Add Annotation (available on the ODS only.)
  • View Annotations (available on the ODS only.)
  • Ack
  • Discard
  • Refresh
 

Audit Viewer

  • Refresh
  • Add Annotation (available on the ODS only.)
  • View Annotations (available on the ODS only.)
  • Clear Audit Log
   

Scheduled Reports (available on the ODS only.)

  • Refresh
   

Tailored Summary Viewer

The menu options available are item-specific (that is, they depend on the type of item selected in the Summary Definitions and Key Data tables).

  • Command
  • Modify
  • Add Annotation (available on the ODS only.)
  • View Annotations (available on the ODS only.)
  • Show Extensions
  • Remove From Site (available for a network engine only).
  • Import Integration (available for a Tailored Summary with trunk/integration data. For example, trunk diagnostics).
  • Command
  • Modify
  • Add Annotation (available on the ODS only.)
  • View Annotations (available on the ODS only.)
 

Trend Viewer

  • Refresh
  • Command

  • Refresh
  • Command
 

Global Search

  • Refresh

  • Refresh
 

Change Results Viewer

No Action menu options for this feature.