Summary of changes - Metasys - LIT-12012458 - Field Device - 13.0

Metasys IP Networks for BACnet/IP Controllers Technical Bulletin

Brand
Metasys
Document type
Technical Bulletin
Document number
LIT-12012458
Version
13.0
Revision date
2023-10-23
Product status
Active
Language
English
The following information is new or revised:
  • Clarified the name of the network architecture tool referenced in Document introduction
  • Added references to OT to highlight differences in IT and OT in Network architecture
  • Updated references to related documentation throughout document