Security - Metasys - LIT-12012458 - Field Device - 13.0

Metasys IP Networks for BACnet/IP Controllers Technical Bulletin

Brand
Metasys
Document type
Technical Bulletin
Document number
LIT-12012458
Version
13.0
Revision date
2023-10-23
Product status
Active
Language
English

Take a least privilege approach regarding network security in the Metasys BACnet/IP network. That is, only allow access to individuals, devices, and protocols that require access to the Metasys BACnet/IP network. Access to the network infrastructure by individuals is restricted through the use of passwords. Access to the switching and routing functions of the network infrastructure is restricted by limiting the number of configured switch ports, and restricting devices and protocols through the use of ACLs.