While other switch vendors may support MRP, Cisco has optimized their MRP ring manager to support large rings of Johnson Controls IP controllers. Cisco is therefore Johnson Control’s switch vendor of choice when deploying MRP rings.
The following steps are required to configure an MRP ring on a Cisco Industrial Ethernet (IE) managed switch.
Configuration Step |
Cisco IE 2000 IOS CLI command |
Cisco IE 3100 IOS XE CLI command |
|
---|---|---|---|
1 |
Enable the MPR ring manager right-to use license. |
|
Active by default in IOS XE. |
2 |
Enter global configuration mode. |
|
|
3 |
Disable PROFINET MRP. |
|
Active by default in IOS XE. |
4 |
Create an MPR ring (1-3). In this example, MPR ring 1 is created. |
|
|
5 |
Configure the MRP manager mode. |
|
|
6 |
Configure the domain ID of the MRP ring. In this example the 32 hexadecimal digit domain ID of MPR ring 1 is set to 1 followed by 31 Fs. |
|
|
7 |
Configure the VLAN of the MRP ring. In this example, the MRP ring is in VLAN 10. |
|
|
8 |
Configure the recovery profile of the MRP ring. In this example, the maximum recovery time is set to 200 msec. |
|
|
9 |
Exit configuration mode for the MRP ring. |
|
|
10 |
Configure the switch port that will serve as the first ring port for the MRP ring. In this example, switch ports 1 and 2 will be configured as the ring ports for MRP ring 1. |
|
|
11 |
Configure the switch port as an access port. |
|
|
12 |
Associate the switch port with the MPR ring. |
|
|
13 |
Exit configuration mode for the switch port. |
|
|
14 |
Configure the switch port that will serve as the second ring port for the MRP ring. |
|
|
15 |
Configure the switch port as an access port. |
|
|
16 |
Associate the switch port with the MPR ring. |
|
|
17 | Exit global configuration mode. |
|