Configuring IP controller device IP ACLs - Metasys - LIT-12012458 - Field Device - 13.0

Metasys IP Networks for BACnet/IP Controllers Technical Bulletin

Brand
Metasys
Document type
Technical Bulletin
Document number
LIT-12012458
Version
13.0
Revision date
2023-10-23
Product status
Active
Language
English
Table 1. Configuring an IP ACL on a Cisco managed switch

Configuration step

Cisco IOS CLI command

1

Enter global configuration mode.

Switch# configure terminal

2

Create an IP ACL for Metasys IP controllers. In this example, the ACL is named JCI-TIER3.

Switch(config)# ip access-list extended JCI-TIER3

3

Allow BACnet in either direction between any devices. In this example, the default BACnet port of 47808 is being used.

Switch(config-ip-acl)# permit udp any any eq 47808

4

Allow messages to DHCP servers in either direction between any devices.

Switch(config-ip-acl)# permit udp any any eq bootps

5

Allow messages to DHCP clients in either direction between any devices.

Switch(config-ip-acl)# permit udp any any eq bootpc

6

Allow ping requests in either direction between any devices.

Switch(config-ip-acl)# permit icmp any any echo

7

Allow ping responses in either direction between any devices.

Switch(config-ip-acl)# permit icmp any any echo-reply

8

Exit global configuration mode.

Switch(config-ip-acl)# end