Dynamically Creatable: No
Dynamically Deletable: No
Property Name |
Required |
Optional |
Proprietary |
Property ID |
Data Type |
Writable |
Range |
---|---|---|---|---|---|---|---|
OBJECT_NAME |
X |
77 |
|||||
OUT_OF_SERVICE |
X |
81 |
X |
||||
STATUS_FLAGS |
X |
111 |
|||||
EVENT_STATE |
X |
36 |
|||||
POLARITY |
X |
84 |
X |
||||
PRESENT_VALUE |
X |
85 |
X |
||||
RELINQUISH_DEFAULT |
X |
104 |
X |
||||
PRIORITY_ARRAY |
X |
87 |
|||||
CURRENT_COMMAND_PRIORITY |
X |
431 |
|||||
ACTIVE_TEXT |
X |
4 |
X |
40 characters max |
|||
INACTIVE_TEXT |
X |
46 |
X |
40 characters max |
|||
COS_TIME |
X |
16 |
|||||
COS_COUNT |
X |
15 |
X |
||||
STATE_COUNT_RESET |
X |
115 |
X |
||||
ELAPSED_ACTIVE_TIME |
X |
33 |
X |
0–4,294,967,295 |
|||
ACTIVE_TIME_RESET |
X |
114 |
X |
||||
MIN_OFF_TIME |
X |
66 |
X |
0–604,800 |
|||
MIN_ON_TIME |
X |
67 |
X |
0–604,800 |
|||
DESCRIPTION |
X |
28 |
X |
40 characters max |
|||
DEVICE_TYPE |
X |
31 |
X |
20 characters max |
|||
RELIABILITY |
X |
103 |
X 1 |
||||
ACKED_TRANSITIONS |
X 2 |
0 |
|||||
EVENT_ENABLE |
X2 |
35 |
X |
||||
EVENT_TIME_STAMPS |
X2 |
130 |
|||||
EVENT_MESSAGE_TEXTS |
X2 |
351 |
|||||
EVENT_MESSAGE_TEXTS_CONFIG |
X2 |
352 |
X |
||||
EVENT_DETECTION_ENABLE |
X2 |
353 | |||||
NOTIFICATION_CLASS |
X2 |
17 |
X |
1–4,194,302 |
|||
FEEDBACK_VALUE |
X2 |
40 |
X |
||||
NOTIFY_TYPE |
X2 |
72 |
X |
||||
TIME_DELAY |
X2 |
113 |
X |
0–65,535 |
|||
ALARM_STATE |
X |
1006 |
Enumerated |
||||
INTRINSIC_ALARMING_DEFINED |
X |
569 |
Boolean |
X |
|||
ENABLED |
X |
673 |
Boolean |
X |
|||
EXECUTION_PRIORITY |
X |
2197 |
Enumerated |
X |
0–3 |
||
ITEM_REFERENCE |
X |
32527 |
Character String |
||||
OBJECT_CATEGORY |
X |
908 |
Enumerated |
X |
0–249 |
||
OFFLINE |
X |
913 |
Boolean |
||||
RESTORE_COMMAND_PRIORITY |
X |
721 |
Bit String |
X |
|||
STATUS |
X |
512 |
Enumerated |
||||
SAB_MAC_ADDR |
X |
3645 |
Unsigned |
||||
SLOT_A |
X |
990 |
Unsigned |
||||
SLOT_B |
X |
991 |
Unsigned |
||||
STATES_TEXT |
X |
931 |
Enumerated |
X |
|||
USER_NAME |
X |
2390 |
Character String |
||||
GRAPHIC |
X2 |
32581 |
Character String |
X |
|||
GRAPHIC_ALIAS |
X2 |
32623 |
Character String |
X |
|||
HEAVY_EQUIP_DELAY |
X |
516 |
Unsigned |
X |
0–255 |
||
HED_CONTROLLER |
X |
517 |
Unsigned |
X |
1–5 |
||
MINIMUM_CYCLE_TIME |
X |
2199 |
Unsigned |
X |
0-65,535 | ||
SETUP |
X |
518 |
Enumerated |
||||
PULSE_WIDTH |
X |
600 | Real |
X |
0-100 | ||
OUTPUT |
X |
663 | Boolean | ||||
ALARM_MESSAGE_TEXT |
X2 |
536 |
Character String |
X |
255 characters |