Networking Options for CGE models only - Metasys - LIT-12013102 - M4-CGM09090-0 - M4-CGE09090-0 - M4-CGM04060-0 - M4-CGE04060-0 - Field Device - M4-CGM General Purpose Application Controller - 11.0

Metasys General Purpose Application Controllers Protocol Implementation Conformance Statement

Product
Controls > Field Controls > M4-CGM General Purpose Application Controller
Document number
LIT-12013102
Version
11.0
Revision date
2022-02-07

Router, Clause 6

   

Annex H, BACnet Tunneling Router over IP

   

BACnet/IP Broadcast Management Device (BBMD)

   
 

Does the BBMD support registrations by Foreign Devices?

Yes

No