Document Introduction - Metasys - LIT-12013102 - M4-CGE04060-0 - M4-CGE09090-0 - M4-CGM04060-0 - M4-CGM09090-0 - Field Device - M4-CGM General Purpose Application Controller - 11.0

Metasys General Purpose Application Controllers Protocol Implementation Conformance Statement

Product
Controls > Field Controls > M4-CGM General Purpose Application Controller
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013102
Version
11.0
Revision date
2022-02-07

This document contains the Protocol Implementation Conformance Statement (PICS) and BACnet® Interoperability Building Blocks (BIBBs) for the Metasys General Purpose Application Controller Series (CG series), as required by the ANSI/ASHRAE Standard 135 for BACnet protocol.

The PICS is a written document created by the manufacturer of a device to identify the particular options specified in the BACnet standard and implemented in the device.

BIBBs are collections of one or more BACnet services. This document includes a listing of the BIBBs currently supported by the M 4-CGM09090-0, M 4-CGM04060-0, M 4-CGE04060-0 and M 4-CGE09090-0 General Purpose Application Controllers.