BACnet Interoperability Building Blocks (BIBBs) (Annex K) - Metasys - LIT-12013102 - M4-CGM09090-0 - M4-CGE09090-0 - M4-CGM04060-0 - M4-CGE04060-0 - Field Device - M4-CGM General Purpose Application Controller - 11.0

Metasys General Purpose Application Controllers Protocol Implementation Conformance Statement

Product
Controls > Field Controls > M4-CGM General Purpose Application Controller
Document type
Protocol Implementation Conformance Statement
Document number
LIT-12013102
Version
11.0
Revision date
2022-02-07

The following table lists all BIBBs that are supported. The table is divided into BIBBs required for the Controller (B-AAC) profile, followed by additional BIBBs that are supported but not required for the Controller profile.

Table 1. BACnet B-AAC BIBBs Support

BIBB Name (A = Initiates and B = Executes)

Designation

Required for B-AAC Profile

Data Sharing - Read Property - B

DS-RP-B

Data Sharing - Read Property Multiple - B

DS-RPM-B

Data Sharing - Write Property - B

DS-WP-B

Data Sharing - Write Property Multiple - B

DS-WPM-B

Alarm and Event Management - Notification Internal - B

AE-N-I-B

Alarm and Event Management- Acknowledge - B

AE-ACK-B

Alarm and Event Management - Information - B

AE-INFO-B

Scheduling - Internal - B

SCHED-I-B

Device Management - Dynamic Device Binding - A

DM-DDB-A

Device Management - Dynamic Device Binding - B

DM-DDB-B

Device Management - Dynamic Object Binding - B

DM-DOB-B

Device Management - Device Communication Control - B

DM-DCC-B

Device Management - Time Synchronization - B

DM-TS-B

Device Management - UTC Time Synchronization - B

DM-UTC-B

Device Management - Reinitialize Device - B

DM-RD-B

Not Required for B-AAC Profile

Data Sharing - Read Property - A

DS-RP-A

Data Sharing - Read Property Multiple - A

DS-RPM-A

Data Sharing - Write Property - A

DS-WP-A

Data Sharing - Change Of Value - B

DS-COV-B

Data Sharing - Change Of Value Property - B

DS-COVP-B

Data Sharing - Change Of Value Unsubscribed - B

DS-COVU-B

Executes ReadRange

Executes ReadRange

Alarm and Event Management - Alarm Summary - B

AE-ASUM-B

Alarm and Event Management - Enrollment Summary - B

AE-ESUM-B

Alarm and Event Management - Event Log - Internal - B

AE-EL-I-B

Alarm and Event Management - Configurable Recipient Lists - B

AE-CRL-B

Scheduling - External - B

SCHED-E-B

Trending - Viewing and Modifying Trends Internal - B

T-VMT-I-B

Trending - Automated Trend Retrieval - B

T-ATR-B

Device Management - Restart - B

DM-R-B

Device Management - List Manipulation - B

DM-LM-B