Technical Specifications - Metasys - LIT-12011527 - Software Application - Metasys Export Utility - 10.0

Metasys Export Utility Installation Instructions

Product name
Metasys Export Utility
Document type
Installation Guide
Document number
LIT-12011527
Version
10.0
Revision date
2018-12-17
Table 1. Metasys Export Utility System Requirements

Product Code

MS-EXPORT-0, MS-EXPORT-6

Required Computer/Server Platform

When Metasys Export Utility is installed on an ADS/ADX or ODS, follow the requirements for an ADS/ADX. Refer to the Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin (LIT-1201525), the Application and Data Server (ADS) Lite-E Product Bulletin (LIT-12011690), or the Application and Data Server (ADS) Lite-A Product Bulletin (LIT-12011694).

When Metasys Export Utility is installed on an Open Data Server (ODS), follow the requirements for an ODS. Refer to the Open Data Server Product Bulletin (LIT-12011943).

Required Memory1

Computer Platforms: 8 GB RAM

Server Platforms: 16 GB RAM

Supported Operating Systems

Windows® 10 Pro and Enterprise Editions with Creators Update (version 1709 or later) (64-bit)

Windows® 8.1 Pro and Enterprise Editions with Update 1 (64-bit)

Windows® 7 Professional, Enterprise, and Ultimate Editions with SP1 (64-bit)

Windows® Server® 2016 (64-bit)

Windows® Server® 2012 R2 with Update 1 (64-bit)

Windows® Server® 2012 (64-bit)

Additional Software Included with Metasys Export Utility

Microsoft .NET Framework version 3.5 SP1

For steps on installing .NET Framework, refer to the Metasys® Server Installation and Upgrade Instructions Wizard (LIT-12012162), Metasys® Server Lite Installation and Upgrade Instructions Wizard (LIT-12012258), or the ODS Installation and Upgrade Instructions Wizard (LIT-12011945).

Note: We recommend you also install Microsoft .NET Framework version 4.5 if you are using Windows 8.1, Windows Server 2012 R2, or Windows Server 2012 and Microsoft .NET Framework version 4.6 if you are using Windows 10.

Additional Requirements (Order Separately)

Microsoft Office 2016, Microsoft Office Professional 2013, Microsoft Office 365, Microsoft Office Professional 2007, or Microsoft Office Professional 2010 software to generate reports

Note:
  • To extract data to Microsoft Excel or Microsoft Access software, you must have the software installed on the computer that is running the Metasys Export Utility.
  • Metasys Export Utility can extract data to 32-bit and 64-bit versions of Microsoft Office. However, the DLL file and example files used to create custom reports are compatible only with the 32-bit version of Microsoft Office.
1 Our computer platform and memory recommendations are not meant to imply that older or slower machines are not usable. Refer to the Network and IT Guidance Technical Bulletin (LIT-12011279) for more information regarding computer or server recommendations.