Overview - Metasys - LIT-12011527 - Software Application - Metasys Export Utility - 10.0

Metasys Export Utility Installation Instructions

Product
Building Automation Systems > Configuration and Programming Tools > Metasys Export Utility
Document type
Installation Guide
Document number
LIT-12011527
Version
10.0
Revision date
2018-12-17

The Metasys Export Utility extracts data from the Metasys system. It runs from an Application and Data Server/Extended Application and Data Server (ADS/ADX), an Open Data Server (ODS), or from a stand-alone computer on the same network.

The Metasys Export Utility extracts historical trend, alarm, and audit data from the Network Automation Engine (NAE)/Network Integration Engine (NIE)/Network Control Engine (NCE), ADS/ADX, or ODS. This data is then provided in several file formats, such as Microsoft Excel® spreadsheet and Access database, as selected by the user. The user can instantly extract the selected data or schedule an extraction at a convenient time or interval.

Note: If you encounter an out-of-memory exception as you export data, select a smaller data set, or increase RAM.