Custom Installation of Metasys Export Utility - Metasys - LIT-12011527 - Software Application - Metasys Export Utility - 10.0

Metasys Export Utility Installation Instructions

Product name
Metasys Export Utility
Document type
Installation Guide
Document number
LIT-12011527
Version
10.0
Revision date
2018-12-17
  1. Obtain the Metasys Export Utility installation file.
  2. Browse to the Metasys Export Utility folder and double-click on MetasysExportUtility.exe.
  3. A User Account Control dialog box appears, click Yes.
  4. Click Custom.
  5. Click Browse to install the Metasys Export Utility in a location other than the default location.
  6. Click Install.
  7. Click Finish if a restart is not needed. Or, before you click Restart Now, go to Activating the Metasys Export Utility License.
  8. After licensing the software, come back to this window and click Restart Now.
    Note: If you are upgrading Metasys Export Utility, see Deleting Leftover Microsoft Excel Files (Upgrade Only).