Changing the Report and Definitions Paths After Install - Metasys - LIT-12011527 - Software Application - Metasys Export Utility - 10.0

Metasys Export Utility Installation Instructions

Product
Building Automation Systems > Configuration and Programming Tools > Metasys Export Utility
Document type
Installation Guide
Document number
LIT-12011527
Version
10.0
Revision date
2018-12-17

Both the default report path and definition path are set by the installer and can be changed during install. If you want to change the path after install, you need to alter the path in the MEUConfig.xml file. To change the paths after install, complete the following steps:

  1. Navigate to the MEU folder. The default location is: C:\ProgramData\Johnson Controls\MetasysIII\MEU
  2. Open MEUConfig.xml.
  3. To change the report path, select the text between the <reportsDirectory> tags. This line is highlighted in Figure 2.
  4. To change the definitions path, select the text between the <definitionsDirectory> tags.
  5. Enter the file path you want to use between the tags.
  6. Save the file.
Figure 1. MEUConfig.xml with reportsDirectory highlighted