Icon right-click menu - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

Use the Metasys Database Manager icon right-click menu to access the Metasys Database Manager and its monitoring settings. The following table outlines the taskbar icon menu options.

Table 1. Taskbar Icon Menu

Selection

Description

Open

Opens the Metasys Database Manager. See Managing databases for more information.

Settings

Displays the Settings window where you can view and modify the monitoring parameters. See Monitoring databases for more information.

View Log File

Launches the Windows Event Viewer. See Log file for more information.

Help

Opens the Metasys Database Manager Help.

About

Displays version information.

Exit

Stops all database monitoring and removes the taskbar icon. To start monitoring again and restore the icon, see Monitoring databases.