Database server - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

The Database Server section displays information on the SQL Server software. The following table outlines the contents of the Database server section.

Table 1. Database Server Section Contents

Field

Description

Server Name

Displays the name of the local running SQL Server software.

Current Database Server Connections

Displays the number of connections to SQL Server software at the time you launch the Metasys Database Manager. If the value of this field is 0, you are using the Metasys Database Manager in a limited capacity (read-only) because the user running the tool is not a SQL Server database administrator.

This value is not refreshed.

Server Type

Displays the type of SQL Server software that has been installed.

For example, this field may contain Express Edition (64-bit).