Statistics tab - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

The Statistics tab contains information about the SQL Server software loaded on the Metasys ADS, ADX, OAS, NAE85, or LCS85 computer and displays database information for each of the trend, alarm (event), audit, annotation, and reporting databases.

The Statistics tab is divided into two sections, as shown in the following figure:

See Status bar for information about the status bar.

Figure 1. Statistics Tab