Maintenance type - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

Use the Maintenance Type section to create a backup before maintenance. The following table outlines the Maintenance Type selections.

Table 1. Maintenance Type Selections

Selection

Description

Manual

Requires you to choose a threshold (see Maintenance thresholds), choose databases (see Database selection), and click Purge Data Now to purge the database.

Note: Currently, this is the only option available to maintain your databases. It cannot be deselected.

Create Backup Prior to Maintenance?

When selected, creates a backup file before data is purged from the databases.

Note: The backup fails if there is not sufficient disk space at the backup destination.