Backup tab - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

The Backup tab allows you to create a SQL Server software backup of a database. If you cannot see this tab, see Required access rights for more information.

The Backup tab is divided into two sections, as shown in the following figure:

See Status bar for information on the status bar.

Figure 1. Backup Tab