Status bar - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

The status bar provides information on the current activity of the Metasys Database Manager and is visible at the bottom of all tabs. The status bar is not present on the Monitoring Settings window.

Figure 1. Status Bar

Table 1. Status Bar Components

Callout

Part

Description

1

Icon

Displays an icon that depicts the status of a Metasys Database Manager action:

- ready

- purging records from a database

- action failed

- refreshing statistics

- restoring a database

- shrinking a database and shrinking database files

- backing up a database

- resetting Internet Information Services (IIS)

- starting the Metasys Device Manager

Note: During some maintenance operations, the Metasys Device Manager shuts down to avoid possible database read/write conflicts. This process restarts the Metasys Device Manager so that the Metasys user interface is once again available to users.

- shutting down the Metasys Device Manager

Note: During some maintenance operations, the Metasys Device Manager shuts down to avoid possible database read/write conflicts. The Metasys user interface is unavailable to users during this time.

- action successful

2

Text

Includes text that describes the action currently taking place. If the Metasys Database Manager is not currently performing a task, this part of the status bar shows when the data was gathered from the database (when the snapshot was taken).

3

Additional Text

Provides additional status description text. For example, when purging records, this part of the status bar displays the number of records deleted from the total number of records.