Settings.xml - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

The Settings.xml file stores settings from both the Metasys Database Manager and the Metasys Database Manager Monitor. The file is stored in the XML directory in the Metasys Database Manager home directory. This file is necessary for proper operation of both applications and should not be moved or removed. Avoid editing the Settings.xml file unless it is necessary.