Warning - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

Use the Warning section to define the warning limit parameters as shown in the following table.

Table 1. Warning Section Contents

Field

Description

Warning File Size Limit

Choose the percentage of the maximum file size that the database file must reach before a warning appears.

Show Warning Reminder every

Select this check box to show a warning balloon when a database size exceeds the value in Warning File Size Limit.

Choose how often you want to show the balloon. By default, every 24th interval is selected, which shows the warning balloon once a day until the database has been reduced to an acceptable level.

Email on Warning

Select this check box to enable the email feature of the Metasys Database Manager Monitor. Only one email is sent when the database exceeds its warning limits.