General - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

The General section contains the main settings for monitoring databases as shown in the following table.

Table 1. General Section Contents

Field

Description

Scan Interval

The frequency with which the databases are checked against their limits. Options are:

  • Every half hour
  • Every hour
  • Every 8 hours
  • Every day

Start Time

The hour and minute that the check on the databases first occurs

Note: For scan intervals of every half hour and every hour, the hour selection is disabled because it is not applicable.

By default, the Metasys Database Manager Monitor checks the databases every hour on the 53rd minute so it does not interfere with the default ADS Delivery Time of 12:15 A.M. ADS Delivery Time is the name of the parameter for an ADS.