Alarm - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

Use the Alarm section to define the alarm limit parameters as shown in the following table.

Table 1. Alarm Section Contents

Field

Description

Maximum File Size Limit

Choose the percentage of the maximum file size that the database file must reach before an alarm appears.

Show Alarm Reminder Every

Select the check box to show an alarm balloon when a database size exceeds the value in Maximum File Size Limit.

Choose how often you want to show the balloon. By default, every interval is selected, which shows the alarm balloon once a day until the database has been reduced to an acceptable level.

Email on Alarm

Select this check box to enable the email feature of the Metasys Database Manager Monitor. Only one email is sent when the database exceeds its alarm limits.