Monitoring settings - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

Use the monitoring capabilities of Metasys Database Manager to set the file size limit in percentage full, that determines the database status. Database statuses are Normal, Warning, and Alarm. Monitoring settings appear in a different window from the tabbed window described in Tabs.

When you log in to the Windows OS on an ADS, ADX, OAS, NAE85, or LCS85 computer, the monitoring starts automatically. Monitoring does not stop unless you exit monitoring or log out of the Windows OS on the ADS, ADX, OAS, NAE85, or LCS85 computer. If you exit and want to restart monitoring, you must either log in to the Windows OS on the ADS, ADX, OAS, NAE85, or LCS85, or restart the monitoring itself. See Stopping database monitoring and Accessing/Starting monitoring settings for information.

Note: If you have administrator privileges, the Metasys Database Manager Monitoring Settings window appears each time you restart your computer, unless you have already configured it for monitoring. See Choosing monitoring settings for more information. To access the setting for other users who have administrator privileges, close the Metasys Database Manager Monitor and log in as Administrator. See Accessing/Starting monitoring settings for more information.

The Metasys Database Manager Monitoring Settings window is divided into five sections as shown in the following figure:

Figure 1. Monitoring Settings Window