Update databases - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active

The Update Databases section shows the databases that are searched during the rename process:

  • JCIHistorianDB - trends

  • JCIEvents - alarms (events)

  • JCIAuditTrails - audits

  • JCIItemAnnotation - annotations

  • MetasysReporting - Metasys Advanced Reporting System

  • JCIReportingDB - Metasys UI Reporting

  • SpacesAuthorization - permissions, dashboard and widget metadata, Advanced Search Reports data, and Announcements data.

This section has Old and New fields where you type the old name and the new name of the Site Director or device. Click the Rename Now button to start the find and replace process of the field contents in the Metasys databases.