Backup file path - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

If you select the Create Backup check box, the databases are backed up before the rename process begins.

The Backup File Path field shows the location where the backup file is saved. By default, backups are created in the same directory as the database files.

Click the Browse button to navigate to a new location for the backup files, however, it is best practice that you keep the default path C:\ProgramData\Johnson Controls\MetasysIII\SQLData.