Rename tab - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

The Rename tab is available only when you are using the Metasys Database Manager in Expert Mode. If you cannot see this tab, see Required access rights.

If the ADS, ADX, OAS, NAE85, or LCS85 computer is renamed in the SCT, use the rename function in Metasys Database Manager to replace the old Site Director name or an old device name in the JCI databases with a new name. For more information on renaming a computer in SCT, refer to the SCT: System Configuration Tool Help (LIT-12011964) .

The Rename tab is divided into two sections, as shown in the following figure:

See Status bar for information on the status bar.

Figure 1. Rename Tab