Expert mode - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

You can view two additional tabs in Expert Mode:

To access Expert Mode, browse to C:\Program Files (x86)\Johnson Controls\Metasys Database Manager, as shown in the following figure. Double-click Expert Mode in the Metasys Database Manager file.

Figure 1. Expert Mode

If you are performing an out-of-place upgrade, use Expert Mode to restore databases and rename database field contents.

Note: Expert Mode functionality does not remain if you close the window and then start the Metasys Database Manager in standard mode.