Verifying the Metasys Advanced Reporting System - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
  1. Click Launch ADX. Log in to the ADX.
  2. Click Next. Select the Tools menu, the select Metasys Advanced Reporting user interface.
  3. Click Next. Log in to the Metasys Advanced Reporting user interface.
  4. Click Next. Verify that the user interface appears correctly and that the site and ADX have the correct name.
  5. Click Next. Verify that the navigation tree that appears in the Metasys Advanced Reporting user interfaces matches that on the SCT/server.
  6. Click Next. Select Alarm Definition Report and click Run.
  7. Click Next. Verify that the report window appears.
    Note: The content of the window is not important at this time. Simply verify that the window opens successfully.
  8. Click Next. Close the report window.
  9. Click Next. Select Event, then select Summary Report. Click Run.
  10. Click Next. Verify that the report window appears.
    Note: The content of the window is not important at this time. Simply verify that the window opens successfully.
  11. Click Next. Close the report window.
  12. Click Completed. The Metasys Rename Assistant closes.