Reinstalling the Metasys software - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
  1. Click MDM Rename. The Metasys Database Manager Window opens.
    1. Click the Rename tab.
    2. In the Old box, enter the Old Site Director name or Old Child Device name. This is found in red text in the pop-up instructions with the Metasys Rename tool.
    3. In the New box, enter the New Site Director or New Child Device name, this is found in red text in the pop-up instructions with the Metasys Rename tool.
      Note: Ensure you use the proper name format. Enter the old value in the following format: SiteDirector:SiteDirector or SiteDirector:Device. Enter the new value in the following format: NewSiteDirector:NewSiteDirector or SiteDirector:NewDevice or .NewSiteDirector:Device.
    4. Click Rename Now.
    5. Close the Metasys Database Manager.
  2. Click Browse under the Install Metasys SCT. The Browse window opens. Navigate to and select the SCT installation file. Click Open.
  3. Click Install. The Metasys SCT installation window opens.
    1. Click Install.
    2. Select the server from the Server Name drop-down. Click Install.
    3. Click Finish.
  4. Click Browse under the Install Metasys Server. The Browse window opens. Navigate to and select the ADS installation file. Click Open.
  5. Click Install. The Metasys Server installer opens.
    1. Click Install.
    2. Select the server from the Server Name drop-down. Click Install.
    3. Click Restart Now.