- Click Backup to open the Metasys Database Manager to back up your
databases. The Metasys Database Manager window opens.
- Select the Backup tab.
- Take note of the backup file path.
- Under Database Selection, choose which database(s) that you would like to back up.
- Click Back Up Now to back up the selected database(s).
- Once backup is complete, close Metasys Database Manager window.
- Select the checkbox that denotes you have performed the Metasys database backup in the Metasys Rename Assistant window.
- Verify the time zone and time for the computer are
correct, and select the checkbox denoting the Time Zone and Time are
correct. Note: If the time zone and time are not both correct, click the refresh button to update them.
- After you have backed up the databases
and corrected the time zone and time, the rename box unlocks. Enter the new
name that you want to assign to the Metasys Server
and click Validate Name. Note:
- The Name field is case sensitive.
- The new name must be different from the original name.
- Click Continue.
Note: A checkmark icon next to each step indicates the step is complete.