During the rename process, Metasys software may be uninstalled and reinstalled;
refer to the installation documents when necessary. Installation documents that may
be required are:
- Metasys Server Installation and Upgrade Instructions (LIT-12012162)
- Energy Essentials Installation Instructions (LIT-12011539)
- SCT Installation and Upgrade Instructions (LIT-12012067)
Note:
Metasys Release 13.0 does not support Energy
Essentials.
- Once you have read the IMPORTANT notice on the screen, select the checkbox.
- Select the Enable SQL Server Authentication checkbox.
- Type your user name and password into the correct boxes.
- Click Test Connection.
- If the
connection is successful,
Connection: Success
appears underneath theTest Connection
button and a check appears to the right of the button. If the connection fails,Connection: Error
appears underneath theTest Connection
button and an x appears to the right of the button. - You cannot proceed if the Test Connection was not successful.
- If the
connection is successful,
- Click Get Started.