- On the Desktop, right-click the Metasys SCT shortcut. Select Delete. Repeat this for the Metasys SMP shortcut.
- Click Next.
- Click Launcher.
- Click Next.
- On the Launcher screen, click the
SMP tab to edit an
existing SMP profile. Note: If you want to edit a SCT profile, select the SCT tab instead of SMP.
- Log in.
- On the Launcher screen, click the
SMP tab to edit an
existing SMP profile.
- Click Next.
- Select the profile whose description you want to edit.
- Click Edit. The Edit screen appears.
- Click Next. In the New Description field, type the new name you selected for the device.
Note: You cannot change the IP address or host name of the device on the Edit screen. To make that change, delete the device, then add the device again.
- Click Next. Click Save.
- Click Next. Recreate shortcuts on the Desktop if required.
- Click Continue.