Choosing monitoring settings - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

About this task

For more information on the contents of the Monitoring Settings window, see Monitoring settings.

To set the Metasys Database Manager monitoring settings:

Procedure

  1. Access the monitoring settings. See Accessing/Starting monitoring settings.
    Note: If the Settings selection or window is not visible, they may not be available to you based on your Windows access rights or because you need to take special steps when you open the window. See Required access rights and Accessing/Starting monitoring settings.
  2. In the General section of the Monitoring Settings window (Figure 1), select how often you would like the databases monitored.
  3. If you would like to send email notifications of status changes, enter an email address in the Email section.
  4. To send a test email to the addresses you entered in Step 3, click Send Test Email.
  5. In the Warning section, define the parameters for a Warning state. If the databases reach the size that you set here, the taskbar icon changes to and the Metasys Database Manager sends an email to the addresses listed in the Email section (if you select Email on warning).
  6. In the Alarm section, define the parameters for an Alarm state. If the databases reach the size that you set here, the taskbar icon changes to and the Metasys Database Manager sends an email to the addresses listed in the Email section (if you select Email on alarm).
  7. In the Database User Account section, enter your SQL Server software login credentials. If you do not enter your credentials here, the Metasys Database Manager uses the credentials used to log in to the ADS, ADX, OAS, NAE85, or LCS85 computer. See Database login.
  8. Click OK.