Accessing/Starting monitoring settings - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

This procedure starts monitoring if you have stopped it and allows access to the settings while monitoring is taking place.

To choose Metasys Database Manager monitoring settings:

  1. Log in as a user with administrator privileges.
  2. If the Settings selection or Monitoring Settings window does not appear, this may be a result of your Windows access rights (see Required access rights). Do the following:
    1. On the Windows Start menu, go to All Programs > Johnson Controls > Metasys Database Manager.
    2. Right-click Metasys Database Manager and then click Run as Administrator.

      If you are not a member of the Administrator group, a credentials box appears. Enter your credentials.

      If you have sufficient privileges, the User Account Control window appears. Click Yes. The Metasys Database Manager icon appears in the taskbar.

    3. Right-click or or in the taskbar and select Settings. The Metasys Database Manager Monitoring Settings window appears.

Go to Choosing monitoring settings for information on choosing Monitoring settings.