Opening the Metasys database manager to manage your databases - Metasys - LIT-12011202 - Software Application - Metasys Database Manager - 13.0

Metasys Database Manager Help

Brand
Metasys
Product name
Metasys Database Manager
Document type
User Guide
Document number
LIT-12011202
Version
13.0
Revision date
2023-08-14
Product status
Active
Language
English

You manage the database and monitor the database using different windows.

To open the Metasys Database Manager:

  1. Do one of the following:
    • On the Start menu, select Programs > Johnson Controls > Metasys Database Manager > Metasys Database Manager.
    • Right-click or or in the taskbar and select Open.
    • Double-click Metasys Database Manager icon on the desktop.
  2. If the User Account Control window appears, click Yes. If you do not click Yes, only the Statistics tab is available. If the User Account Control window does not appear and the Metasys Database Manager opens with only the Statistics tab available, verify your Windows access rights. See Required access rights.

Go to Checking database statistics, Purging a database, or Backing up a database.