Updating the names of field points - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

About this task

To rename the field points that propagate from a selected node, complete the following steps:

Procedure

  1. From the All Items tree, select the node.
  2. Right-click the selected node, and click Update Field Point Name.
  3. From the list of rules, select the appropriate naming convention.