New file tab - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

You can use the new file tab to configure the default setting for new files based on NIEx9 integrations related to ID rule and alarms, trends, and totalizations extensions.

Use the default values section to specify the ID and Name of the extensions added directly into the MCT. When you perform a reset extensions unique ID operation on a object, the ID restores to the value you set here. You can also specify the default values of the attributes related to field devices, field points, and extensions created in the new file window.