General tab - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document type
User Guide
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24
Table 1 describes the General tab settings.
Table 1. General tab settings
Setting Description
Language Specifies the user interface language.
Dictionary Version Specifies the enumerations dictionary version.
Attributes Order Specifies the order of the attributes in the filters combo.
Objects per IMP file Specifies the maximum number of objects in a file, when split.
Restore Point Period Specifies the period of the restore point creation in minutes. To disable this fiction, set the restore point to 0.
Create Backup file when saving Select this check-box to create a backup file every time you save a file.
Create log file when saving Select this check-box to create a log file every time you save a file.