Model tab - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

You can use the model tab to import an existing IMP file and create a list of models in a table. From the table, you can select a model to view its related objects in the points tree. From the points tree, you can choose the objects or a subset of objects that you want to include in the final IMP file. You can include a subset of field points with the field device object excluded, in the final IMP file.