General tab - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24
You can use the general tab to select the model and integration type of the supervisory device and set naming rules for the creation of devices, field points, and extensions. The rules related to the field devices are based on three key parts: supervisory key (sss), model key (MMM), and device key (ddd). The key fields are highlighted in orange. Table 1 outlines the General tab settings.
Table 1. General tab settings
Setting Field Description
Supervisory Device Key (sss) Defines the supervisory key for naming the field devices.
Model Provides a list of model types for the supervisory device.
Integration Provides a list of integration types for the supervisory device.
Rules Controllers Unique ID Defines the naming rule to apply to the controllers unique ID.
Controllers Name Defines the naming rule to apply to the controller names.
Field Point Name Defines the naming rule to apply to field point names.
Extension Defines the naming rule to apply to the extension names.