You can use the general tab to select the model and integration type of the
supervisory device and set naming rules for the creation of devices, field points, and
extensions. The rules related to the field devices are based on three key parts:
supervisory key (sss), model key (MMM), and device key (ddd). The key fields are
highlighted in orange. Table 1 outlines the General tab settings.
Setting | Field | Description |
---|---|---|
Supervisory Device | Key (sss) | Defines the supervisory key for naming the field devices. |
Model | Provides a list of model types for the supervisory device. | |
Integration | Provides a list of integration types for the supervisory device. | |
Rules | Controllers Unique ID | Defines the naming rule to apply to the controllers unique ID. |
Controllers Name | Defines the naming rule to apply to the controller names. | |
Field Point Name | Defines the naming rule to apply to field point names. | |
Extension | Defines the naming rule to apply to the extension names. |