Devices tab - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

You can use the device tab to define the devices in the final IMP file. Each device contains generic attributes that you must define, for example, the ID, name, and description attributes. Depending on the selected integration type, you must define device attributes according to the field device settings. You can exclude a device from the final IMP file and also retain it in the list for future use.