Rapid IMP file creation - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: Tools > Additional Functions > Rapid IMP File Creation

You can use the rapid IMP file creation function to create an IMP file containing multiple devices. The creation of the devices is based on the concept of models. Models are generated when you import IMP files.