Opening the peer to peer viewer - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

About this task

The peer to peer viewer provides the ability to load several CAF files, related to the FEC and NCE controllers and display all the configured peer to peer in a table. The peer to peer viewer highlights errors, for example, peer to peer on the same variable or circular references.

Procedure

  1. Click Tools > Additional Functions > Peer To Peer Viewer.
  2. In the Peer To Peer Viewer window, click File > Load.
  3. Locate the CAF files related to FEC and NCE controllers, and click Open.