Exports from SCT - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

Menu Selection: Tools > Additional Functions > Export from SCT

The export from SCT function provides different options to create reports directly from the SCT database. You can use the export objects list from SCT option to create Excel files containing objects. From the columns you can select the objects you want to include in the Excel files. A file for each supervisory device NAE/NIE/SNx or server ADS/ADX is created. The base files produced leave the enumeration fields, for example, category and states text, as numbers. To replace enumeration fields with the correct localized text, select the translate and localize check-box. To create a statistics file, select the statistics only check box.
Note: If you select the translate and localize option, the length of time to generate the Excel file increases.