Extracting a compressed export database file - Metasys - LIT-12013963 - Software Application - Mass Changes Tool - 3.0.0.x

Mass Changes Tool (MCT) Help

Product
Building Automation Systems > Configuration and Programming Tools > Mass Changes Tool
Document number
LIT-12013963
Version
3.0.0.x
Revision date
2022-06-24

About this task

You can use the extract compressed database function to extract the files in an exported DBEXPORT file and edit the contents. The extracted DBEXPORT file contains individual folders related to a specific supervisory device or server. To extract a compressed database, complete the following steps:

Procedure

  1. Click Tools > Additional Functions > Database Export > Extract Compressed Database.
  2. Locate the DBEXPORT file you want to extract, and click Open.
  3. Select the file storage location, and click OK.